Air Conditioning (AC) Unit Control
Air-conditioning (AC) Unit Control widget provides quick access to the below AC parameters:
-
Power status
-
Operation mode
-
Fan speed
-
Temperature setpoint
To operate the AC Unit Control:
-
Click power button to turn on/off the widget.
-
When the plant is ON, all AC controls such as MODE, FAN SPEED, and TEMPERATURE become active.
-
When the plant is OFF, you can still configure MODE, FAN SPEED, and TEMPERATURE (pre-staging). The Air Conditioner will start with these configured settings when the plant is turned ON.
-
-
Click
/
to increase/decrease the set temperature.
You can set the desired temperature that the AC unit should maintain. The updated temperature value is displayed on the screen.
NOTE: Temperature setpoint can be adjusted only when the mode is set to COOL, HEAT, DRY, or AUTO. It cannot be adjusted when the mode is set to VENT, EXHAUST, PUMP, or any other custom mode. -
Click
/
to increase/decrease the fan speed.
You can adjust the fan speed level supported by the AC unit. The updated fan speed is displayed on the screen.
The fan speed options displayed depend on the supported levels reported by the connected HVAC system and configured in the fan speed object. The Manager interface reads the fan speed object and displays the available levels exactly as defined in the configuration. Common fan speed levels include:
-
LOW
-
MEDIUM
-
HIGH
-
AUTO
-
BOOST
-
QUIET
-
TURBO
NOTE: Fan speed can be adjusted only when the mode is set to COOL, HEAT, DRY, AUTO, or VENT. It cannot be adjusted when the mode is set to EXHAUST, PUMP, or any other custom mode. -
-
Refer the below table for mode icons:
-
Select the required operating mode from the available options.
You can change the operation mode during normal operation. You can also change the mode when the plant is OFF; however, the change will reflect when the plant is turned ON.
The updated mode is displayed on the screen.
The operating modes displayed depend on the modes supported by the connected HVAC system and configured in the mode object. The Manager interface reads the mode object and displays the available modes exactly as defined in the configuration. Common available modes are listed below:
-
COOL
-
HEAT
-
VENT
-
DRY
-
AUTO
-
EXHAUST
-
PUMP
-
-
Refer the below table for other controls:
Controls
Description
Current temperature (Read Only)
Displays the real-time temperature reading from the configured temperature sensor.
Plant Humidity (Read Only)
Displays the value for monitoring the ambient humidity level in the conditioned space.
Plant Humidity is used to:
-
Provide environmental information along with temperature readings.
-
Support HVAC monitoring or automation scenarios if humidity control is required.
-
Example: You can use the AC Unit Control widget to remotely manage your Air Conditioner. Turn it on and set your preferred temperature before you arrive home, so you walk into a cool and comfortable room.