Air Conditioning (AC) Unit Control
Available controls may vary depending on the HVAC system and the configuration performed in the Configurator.
To configure AC Unit Control:
-
In General tab, enter the Title of the widget.
NOTE: Once you select the objects in the Objects tab, based on the configuration defined in the Configurator, the corresponding values will be displayed in the Setpoint step, Temperature Unit, Setpoint minimum value, Setpoint maximum value fields, as well as in the Fan Speeds and Operation Modes sections. -
In the Objects tab, select the Plant On/Off, Operation mode, Fan speed, Current temperature, Plant Humidity and Set Point objects from the drop-down list.
NOTE: Only the objects that have been created and configured in the Configurator will appear in the drop-down list for selection.Refer the below table for field description:
Field
Description
Plant On/Off*
Select the C‑Bus object that represents the HVAC plant ON/OFF status.
Operation mode*
Select the C-Bus object that defines the operating mode of the AC unit.
Fan speed*
Select the C-Bus object to control the fan speed of the AC unit.
Current temperature
Select the C-Bus object that provides the current temperature reading from the connected temperature sensor.
Plant Humidity
Select the C-Bus object that provides the current humidity level.
Set Point
Select the C-Bus object to define the desired temperature setpoint for the AC unit.
TIP: Fields marked with an asterisk (*) are mandatory.
Refer to the table below for supported object type mappings.
Object Field
Supported Object Types
Plant On/Off
All Lighting objects without a specific function (legacy objects), Boolean, and User parameter (Boolean).
Operation Mode
All Lighting objects without a specific function (legacy objects), and User parameter (Integer).
Fan Speed
All Lighting objects without a specific function (legacy objects), Cycle/Fan, User parameter (Integer).
Current Temperature
Measurement application, Unit parameter, and User parameter (Float/Integer).
Current Humidity
Measurement application, and User parameter (Float/Integer).
Setpoint Temperature
All Lighting objects without a specific function (legacy objects), and Measurement application.
Once you select objects in the Objects tab, the values in General section will be displayed.
NOTE: By default, Enabled toggle button is turned on. To deactivate the required Fan speeds and Operation Modes, you can disable the Enabled toggle button. -
In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).
-
Click Save to create the widget.