Software Version 2.14.0

C-Bus Devices

The C-Bus Devices in each network allow you to add C-Bus unit devices in the project.

Add C-Bus Device

Prerequisites: Make sure your project is Open, and network has been selected.

  1. Select the network of the project you want to add unit devices.

  2. On selecting C-Bus Devices, LIBRARY and WORKSPACE window contents are displayed.

    NOTE: Make sure you have LIBRARY and WORKSPACE windows opened.
  3. In the Library window, select the unit device and click .

    This will add device to the project which is displayed in WORKSPACE in Devices in Project section.

    TIP: Alternate ways to add devices:
    • Double-click on unit device

    • Drag and drop unit device to Devices in Project

    IMPORTANT:
    • When the same unit device is added “N” times, each device postfixes with an incriminated number to maintain the uniqueness.

    • Each device can be renamed in their respective Property window (It is advised to rename the device appropriately).

    Each C-Bus device can be configured by making changes in the respective Property window, which can be seen based on the Unit Type categories.

IMPORTANT: In an existing Project, when a C-Bus Device node is clicked the existing device name in Devices in Project is assigned automatically as per following:

If PART NAME is

”NEW UNIT”

If TAG NAME is

“NEW UNIT”

DEVICE NAME is assigned same as Catalog number

If DEVICE NAME is unique in network node

TAG NAME is same as DEVICE NAME

PART NAME is assigned same as DEVICE NAME (maximum 8 characters)

If DEVICE NAME is not unique in network node

Numeric 1 is appended to DEVICE NAME

not “NEW UNIT”

DEVICE NAME is assigned same as TAG NAME

If DEVICE NAME is unique in network node

PART NAME is assigned same as TAG NAME

If DEVICE NAME is not unique in project

PART NAME is assigned same as TAG NAME

Numeric 1 is appended to DEVICE NAME and is incriminated for next instance

is not ”NEW UNIT”

If TAG NAME is

“NEW UNIT”

If PART NAME is

unique in C-Bus network

DEVICE NAME is assigned same as PART NAME

TAG NAME is assigned same as DEVICE NAME

not unique in C-Bus network

Numeric 1 is appended to DEVICE NAME and is incriminated for next instance

DEVICE NAME is assigned same as PART NAME.

not “NEW UNIT”

If TAG NAME is

unique in C-Bus network

DEVICE NAME is assigned same as TAG NAME

not unique in C-Bus network

Numeric 1 is appended to DEVICE NAME and is incriminated for next instance

DEVICE NAME is assigned same as TAG NAME

Add multiple C-Bus devices

Prerequisites: The project must already be opened in EXPLORER window with a network created in the project.

The LIBRARY window allows to add multiple devices at a time.

  1. Select the C-Bus Device of a network in the EXPLORER window

    Step result: The devices that can be added to the network appear in the LIBRARY window .

  2. Select the device and click drop-down, choose Add Multiple.

    TIP: Alternate method to add multiple devices:
    • Right click on the device, and select Add Multiple.

  3. Fill in the device information as demonstrated below:

Add Dali Devices

Prerequisites: A project must already be open in the Explorer window. A network must already be created with a DALI-2 Gateway added to the network, see Add DALI-2 gateway

  1. Select a DALI line in the Explorer window

  2. Select the Dali device and click in Library window

    TIP: Alternate ways to add DALI devices:
    • Double-click on unit device

      or

    • Drag and drop a unit device to Devices in Project

    Step result: Selected device is added to the project.

The different DALI ECG devices in each DALI Line are as listed below:

Device Type

Device Name

Meaning

Emergency or Exit Light DALI ECG DT1 (Generic) Emergency or Exit Light (Generic)
DALI ECG DT1 A Emergency or Exit Light (Switched Maintained Dimmable)
DALI ECG DT1 B Emergency or Exit Light (Switched Maintained Non-Dimmable)
DALI ECG DT1 C Emergency or Exit Light (Maintained)
DALI ECG DT1 D Emergency or Exit Light (Non – Maintained Dimmable)
LED DALI ECG DT 6 Single Channel LED Device
DALI 2x ECG DT 6 DALI 2 Channel Device (DT6)
DALI 3x ECG DT 6 DALI 3 Channel Device (DT6)
DALI 4x ECG DT 6 DALI 4 Channel Device (DT6)
Channel DALI ECG DALI ECG (Generic)
DALI 2x ECG DALI 2 Channel Device (Generic)
DALI 3x ECG DALI 3 Channel Device (Generic)
DALI 4x ECG DALI 4 Channel Device (Generic)
Color Control DALI ECG DT8 Single Channel Tunable / Color Controllable Device
NOTE: When a DALI channel device is added, based on the number of channels DALI device is added. Each DALI channel device can be collapsed and expanded.

Example, when the DALI 3x ECG DT6 is added the result is as shown below:

To Configure DALI ECG Devices, see DALI ECG devices


Add multiple Dali devices

Prerequisites: A project must already be open in the Explorer window. A network must already be created with a DALI-2 Gateway added to the network. A DALI Line must already be selected.

  1. Select the DALI device and click drop-down, choose Add Multiple.

    Step result: Add Multiple DALI Devices dialog box is displayed.

  2. Fill in the device information as demonstrated below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.