Software Version 2.14.0

Network Devices

The Network Devices section displays the devices physically connected to the C-Bus Network, provided a C-Bus Interface is connected to the C-Bus Network and the software is able to communicate to this interface.

The DALI devices will be displayed when a DALI line is selected, provided the C-Bus DALI- 2 Gateway is part of the C-Bus Network.

NOTE:
  • The C-Bus Network must be opened and scanned to display the C-Bus Devices on the Network.

  • The DALI line must be scanned to display the DALI devices on the selected DALI line (DALI-2 Gateway must be reconciled before scanning the DALI line).

Fields

Description

Status

This field displays firmware update icon for the C-Bus Devices indicating a new firmware is available for a respective C-Bus Device and an upgrade is advised.

Address (Addr)

This field displays the unit address assigned to the device.

NOTE:
  • For a C-Bus Device, the values vary from 0 to 255.

  • For a DALI device, the values vary from 0 to 63.

Part Name

This field displays a 8 characters long name that is stored in the device given by the user.

Unit Type

This field displays the unit type of the device on the network.

Catalogue

This field displays the commercial reference for the device.

Description

This field displays the description of the device and cannot be edited.

Serial

This field displays the serial number that is on the physical device which is unique to all the devices.

Firmware

This field displays the version number of the of the physical device. Some devices have multiple firmware’s: interface board, main board.

By default, here the software will display the Main board firmware.

Exists in Project

This field displays whether there is a matching device that exist on the network.

Matching rules:

  1. Yes: Fully matched, where the unit address, serial number, unit type and firmware version are the same in project and on the network.

  2. Unit Type Only: Partial matched, where the unity type, firmware and unit address are the same in project and on the network.

Application

This field displays the selected device's application address that the device has been assigned.

Voltage

This field displays the voltage of the device.

The operations that can be performed in this section are:

  • Open C-Bus network

  • Open C-Bus Network Using Open Using Feature

  • Scan C-Bus devices

  • Transfer device from network to project

  • Sort line/network devices

  • Unravel

  • Readdressing

  • Dynamic Mode Devices

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.