Software Version 2.14.0

Paste Test Groups

The Emergency Exit Light application Test Group Addresses copied from one network are pasted either into another Emergency Exit Light application of a different network.
Prerequisites: The Test Group Address must be already copied from an application.
NOTE: The Emergency Exit Light application Test Group Address copied from one network must be pasted only into the Emergency Exit Light application on another network.
  1. Select the Emergency Exit Light application of the network to be pasted in
  2. Click in the Test Group section
    NOTE: The process to Paste the Test Groups from excel is similar to as demonstrated in lighting application, click here
IMPORTANT: Paste conflict occurs when already existing test group address and test group name are been pasted in emergency exit application of another network.

The process to Resolve conflict is similar to as demonstrated in lighting application, click here

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.