Software Version 2.14.0

Delete Levels

The delete option allows you to delete one or more levels added to a group address.
Prerequisites: The Levels must already be added in the group address.
  1. Select the group address check box. The Levels for the selected group address is displayed.
    NOTE:
    • A single level can be chosen by selecting the check box of the required level, whereas all levels can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one level, then hold down the SHIFT key and select on additional levels (grid) using the mouse.

    • For random multiple selection, select one level, then hold down the CTRL key and select the next levels (grid) using the mouse.

    • The icon will be disabled, if a level is not selected.

  2. Click in the Levels section. A Confirmation pop-up is displayed.
  3. Click Yes to delete the levels.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.