Software Version 2.14.0

Add Enable Group

Prerequisites: The Enable application must be selected in the created network.
  1. Select a network from the EXPLORER window.
  2. Click Applications drop-down.
  3. Select Enable.
    Step result: Respective Enable Groups and Values section of Enable is displayed in the WORKSPACE window.
  4. Click in the Enable Groups section.
  5. Choose address.

    Step result: A Enable Group is created.

    The process to create multiple enable groups at a time is similar to as demonstrated in Lighting Application , click here.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.