Software Version 2.14.0

Copy Test Groups

Prerequisites: The Test Group Addresses must be already created in an application.

The Test Group Addresses in the Emergency Exit Light application can be aligned/arranged with same addresses as in the other Emergency Exit Light application.

  1. Click Emergency Exit Light application.
  2. Select the test groups in the Test Groups section.
    NOTE:
    • A single test group can be chosen by selecting the check box of the required group, whereas all test groups can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one test group, then hold down the SHIFT key and select on additional test group (grid) using the mouse.

    • For random multiple selection, select one test group, then hold down the CTRL key and select the next test group (grid) using the mouse.

      The copy option will be disabled, if a group is not selected.

  3. To copy the selected groups, click in the Test Groups section of Emergency Exit Light application.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.