Software Version 2.14.0

Output Units

The output units control the electrical power going to lighting or other electrical devices such as fans and motors. These units fall into categories that are strongly related to the electrical devices which they power, such as relays and dimmers. Relays are designed to control fluorescent bulbs and other non-dimming electrical devices. Dimmers are designed to accommodate electrical devices which use dimming.

The Devices under Output unit category is as listed below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.