Software Version 2.12.0

Sort Error Objects

Prerequisites: The Error objects must already have been created in theError application.

The existing error objects in application can be sorted.

  1. Select the error object.

    NOTE:
    • A single error object can be chosen by selecting the check box, whereas all error objects can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one error object, then hold down the SHIFT key and select on additional error objects (grid) using the mouse.

    • For random multiple selection, select one error object, then hold down the CTRL key and select the next error objects (grid) using the mouse.

  2. Click in the Device Channel List and Error Details section.

    The available sort methods are displayed.

  3. Select the appropriate sort method. The error object list will be sorted according to the selected sort method.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?