Software Version 2.14.0

Copy Levels

Prerequisites: The Levels must already be added in a Group.

The levels created in a group can be copied from the other group in the same Lighting application on same network or from the Lighting application from different network in the project.

  1. Click Lighting application.
  2. Select the group check box in the Groups section. The Levels for the selected Group are displayed in the Levels section.
  3. Select the required levels and click from Levels section.
    NOTE:
    • A single level can be chosen by selecting the check box of the required level, whereas all levels can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one level, then hold down the SHIFT key and select on additional levels (grid) using the mouse.

    • For random multiple selection, select one level, then hold down the CTRL key and select the next levels (grid) using the mouse.

    • The icon will be disabled, if a level is not selected.

    Step result: The selected levels are copied.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.