Software Version 2.14.0

Paste Values

The paste option allows the user to paste the Values copied from one Enable Group into different Enable Group on the same network or into a Enable Group on another network.
Prerequisites: The Values must already be copied from a Enable Group.
  1. Select a Enable Group in Enable Group section
    NOTE: Values can either be pasted on same network or into a Enable Group on another network/project.
  2. Click in the Values section.
    NOTE: The Process to Paste Values from Excel is similar to as demonstrated in lighting application, click here

    Step result: The copied Values are pasted.

IMPORTANT: Paste conflict occurs when already existing Values name and Values address are been pasted in Enable application.

The process to Resolve conflict is similar to as demonstrated in lighting application, click here

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.