Software Version 2.14.0

Settings

The Settings option allows you to perform general settings for the software, C-Bus and DALI system. The sections in the Settings option are as follows:

To Open Settings

  1. Click .

  2. Select Settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.