Software Version 2.14.0

Edit Levels

Prerequisites: The Levels must already be existing in the selected group of Lighting application.

  1. Double-click on the level name that has to be edited/renamed

    Step result: Edit Group Dialog box is displayed.
  2. Edit the Level name and click OK.

    NOTE: Special characters except /,”,# and maximum of 32 characters in the group name is acceptable.

    Step result: The level name is updated.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.