Software Version 2.14.0

Copy Values

The values created in a Enable Group can be copied from another Enable Network Variable in the same Enable application on same network or from the Enable application from a different network in the project.
Prerequisites: The values must already be copied from a Enable Group.
  1. Click Applications > Enable.
  2. Select the Enable Group.
    Step result: The values for the selected Enable Group are displayed in the Values section.
  3. Select the value check box to be copied in the Values section.
    NOTE:
    • A single value can be chosen by selecting the check box of the required value, whereas all values can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one value, then hold down the SHIFT key and select on additional values (grid) using the mouse.

    • For random multiple selection, select one value, then hold down the CTRL key and select the next value using the mouse.

    • The icon will be disabled, if a value is not selected.

  4. Click in the Values section of Enable Group application.
    NOTE: To copy the complete application, click in the Values section.
    Step result: The selected values are copied.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.