Software Version 2.14.0

Add Test Groups

Prerequisites: The Emergency Exit Light application must be selected in a created network.
  1. Click Applications drop-down in the Explorer window
  2. Click Emergency Exit Light
  3. Click on test group section

    Step result: A test group object is added.

    NOTE:
    • The test group object can be deleted during creation/adding itself using “x” as shown below:

    • The Channel and Device name of the test group object can be modified. Double-click on the channel/device name, edit the device name to match your device and channel name to match the channel that is been monitored on the device, then click enter ( or on the empty space of the section ) to update the change.

  4. The process to create multiple test group objects at a time is similar to as demonstrated in lighting application, see Add multiple test group
    Step result: Multiple test groups are created.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.