Software Version 2.14.0

Delete Values

The delete function allows you to delete one or more values added to a Enable Group.
Prerequisites: The values must already be created in a selected enable group address.
  1. Click Application > Enable.
  2. Select the Enable Group.
    Step result: The values for the selected Enable Group are displayed in the Values section.
  3. Select the Value check box to be deleted in the Values section.
    NOTE:
    • A single value can be chosen by selecting the check box of the required value, whereas all values can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one value, then hold down the SHIFT key and select on additional values (grid) using the mouse.

    • For random multiple selection, select one value, then hold down the CTRL key and select the next values (grid) using the mouse.

    • The icon will be disabled, if a value is not selected.

  4. Click in the Values section. A Confirmation pop-up is displayed.
  5. Click Yes to delete the values.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.