Software Version 2.12.0

Voltage Free Relays

Unit Types

  • RELDN4A - 5504RVF - 4 Channel, 16A DIN Rail Voltage Free Relay, Switchable C-Bus Power Supply

  • RELDN8A - 5508RVF - 8 Channel, 16A DIN Rail Voltage Free Relay, Switchable C-Bus Power Supply

  • RELDN16A - 5516RVF - 16 Channel, 16A DIN Rail Voltage Free Relay, Switchable C-Bus Power Supply

To enable/disable Inbuilt C-Bus Power Supply function for the Voltage Free Relays, click here.

The field information to configure SpaceLogic C-Bus Relay is as explained below:

Applications

This section displays the lighting applications supported by the relays. Up to four lighting applications can be defined and then used throughout the configuration of the relays.

Channels

NOTE:

  • RELDN16A will have 16 channels

  • RELDN8A will have 8 channels

  • RELDN4A will have 4 channels

Group

This field allows to program group addresses associated with relay channels.

You can:

  • Select group address using drop-down list

    .
  • Modify group address using

    .
  • Add group address using .

  • Create a new group name which takes the next available address (it’s a fast commissioning option).

Channel Name

This field allows to define the channel name of the relay.

Channel Location

This field allows to define the channel location of the relay.

Advanced

Turn on Threshold (C-Bus Level)

The turn on threshold has a range of 0 – 255 which are C-Bus levels.

Warn Before off Time

This field allows to set the warn before off time. Warn Before off Time can be set between 1– 15 min.

By default, it is Not Enabled.

Once Warn Before off Time is set, Warn Before off Level field is displayed and enabled to set the range between 1–100 %.

Power Recovery

This field allows to set the power recovery percentage.

By default, it is Restore To Previous.

Restrike Delay

This field defines a time between a channel switching off and switching on. Delay is set in minutes:seconds.

This setting is also applicable for upon device power up.

Mouse over on the Restrike Delay info icon to view the tooltip message.

Logic

Type

This field allows to select the type of the logic group.

Logic Group

This field allows to program logic group addresses associated with relay channels.

You can:

  • Select group address using drop-down list.

  • Modify group address using .

  • Add group address using .

  • Have maximum 4 logic groups.

Mouse over on the Logic info icon to view the tooltip message.

Interlock Channels

The Relay interlock allows interlocking of multiple relay channels, so that only one relay in a group of interlocked relay is On at any one time.

Add Interlock Set

NOTE: The maximum number of interlock sets added depends on the number of Channels assigned to the set.

Example: Having 2 interlock sets added. If set 1 is assigned with 6 channels, then set 2 can be assigned with only the remaining 10 channels.

Click to add new channel interlock set.

Number of channels to interlock is maximum 16, minimum is 2.

Each selected channels in a interlock set can be assigned with highest to lowest priority.

NOTE: No Channel Interlock, when interlock channels are not added No Channels Interlocked is displayed.

Interlock Sets

Each created interlock sets has the mentioned fields

Click to remove an created interlock set.

Interlock Switching Delay (sec)

Allows to set the seconds of delay for interlock switching between the range 0.1 to 10 sec.

Mouse over on the Interlock Switching Delay (sec) info icon to view the tooltip message.

Number of channels to Interlock

Select the number of channels to interlock (2, 3, 4).

High Priority

Select the channel to set as an highest priority and allocate the percentage.

Click to remove the assigned priority.

Lowest Priority

Select the channel to set as an lowest priority and allocate the percentage.

Click to remove the assigned priority.

Remote On/Off

This field allows to choose the combinations of Remote On and Off for each individual channels.

NOTE :

  • RELDN16A will have 16 channels

  • RELDN8A will have 8 channels

  • RELDN4A will have 4 channels

Error Reporting

This section display the fields for error reporting

Device ID

This field displays the unit address of the device.

NOTE: The Device ID is for the entire device and is as same for Measurement section.

When you assign a Device ID, and if you set the Device ID to Not Assigned, then all properties in both the Error Reporting and Measurement section are reverted to their default settings and disabled (grey out state).

Mouse over on the Device ID info icon to view the tooltip message.

Mode Control Group

This field allows to add an enable group (0–254).

If you assign a group, Restore To Previous field is displayed and Regular Reporting Interval drop-down is enabled.

If you uncheck the Restore To Previous check box, Regular Reporting field will be enabled.

If you check Restore To Previous check box, Regular Reporting will be disabled.

Regular Reporting

This field configures the Error Reporting mode of the relays into one of the below modes:

  • Disabled (Triggered only): Errors are reported only when triggered by the assigned Trigger Group.

  • All Errors, most recent only (Mode 1): The most recent errors are reported automatically at a regular time interval (time set by the Regular Report Interval field).

  • All Errors, most recent and most severe (Mode 2): The most recent and most severe (or latched) errors are reported automatically at a regular time interval (time set by the Regular Report Interval field).

  • Minimum Errors, most recent only (Mode 3): The most recent minimum errors are reported automatically at a regular time interval (time set by the Regular Report Interval field).

  • Minimum Errors, most recent and most severe (Mode 4): The most recent and most severe minimum errors are reported automatically at a regular time interval (time set by the Regular Report Interval field).

All the modes can be set with the regular reporting interval set to No regular reports, which allows live reporting of errors without the regular reports.

Mouse over on the Regular Reporting info icon to view the tooltip message.

Restore to Previous

If selected, this field restores the data on power failure.

When you click Save with the below conditions:

  • Mode Control Group — Assigned

  • Restore to Previous — Checked

  • Regular Reporting — Disabled state

The Regular Reporting displays the last saved value.

Mouse over on the Restore to Previous info icon to view the tooltip message.

Regular Reporting Interval

This field is used to select the time interval period between the completion of a regular report and beginning of the next report in Always On, Most recent only and Always On, Most recent and most severe modes. By default, the interval is 30 minutes.

Regular Reporting Interval is enabled for Trigger Only mode.

Trigger Group

This field contains a Trigger Group to trigger an error reporting event for any of the three error reporting modes. When a Trigger group is created, Resend Action Selector and Acknowledge Action selector fields are displayed.

The Resend Action Selector is set to send all errors and Acknowledge Action selector is set to acknowledge all errors.

Destination Network

This field contains the destination C-Bus network to which the relays routes the error reporting messages. This allows the error messages to be sent to a remote C-Bus network for central monitoring if it’s not the local network.

Mouse over on the Destination Network info icon to view the tooltip message.

Advanced

C-Bus Voltage Warning Set Threshold

  • By default, Disabled is selected.

  • The value selected must be less than the C-Bus Voltage Warning Clear Threshold value selected.

  • If the C-Bus Voltage Warning Clear Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Warning Clear Threshold value to (current C-Bus Voltage Warning Set Threshold value + 1 V).

Mouse over on the C-Bus Voltage Warning Set Threshold info icon to view the tooltip message.

C-Bus Voltage Warning Clear Threshold

  • By default, Disabled is selected

  • The value selected must be greater than the C-Bus Voltage Warning Set Threshold value selected.

  • If the C-Bus Voltage Warning Set Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Warning Set Threshold value to (current C-Bus Voltage Warning Clear Threshold value - 1 V).

Mouse over on the C-Bus Voltage Warning Clear Threshold info icon to view the tooltip message.

C-Bus Voltage Critical Set Threshold

  • By default, Disabled is selected

  • The value selected must be less than the C-Bus Voltage Critical Clear Threshold value selected.

  • If the C-Bus Voltage Critical Clear Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Critical Clear Threshold value to (current C-Bus Voltage Critical Set Threshold value + 1 V).

  • If the C-Bus Voltage Warning Set Threshold has a value set (other than Disabled), then the value selected must be less than (current C-Bus Voltage Warning Set Threshold value).

Mouse over on the C-Bus Voltage Critical Set Threshold info icon to view the tooltip message.

C-Bus Voltage Critical Clear Threshold

  • By default, Disabled is selected

  • The value selected must be greater than the C-Bus Voltage Critical Set Threshold value selected.

  • If the C-Bus Voltage Critical Set Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Critical Set Threshold value to (current C-Bus Voltage Critical Clear Threshold value - 1 V).

Mouse over on the C-Bus Voltage Critical Clear Threshold info icon to view the tooltip message.

C-Bus Power Supply Warning Set Threshold

  • By default, Disabled is selected.

  • The value selected must be greater than the C-Bus Power Supply Warning Clear Threshold value selected.

  • If the C-Bus Power Supply Warning Clear Threshold is Disabled, then setting a value here will also set the C-Bus Power Supply Warning Clear Threshold value to (current C-Bus Power Supply Warning Set Threshold value - 10 mA).

Mouse over on the C-Bus Power Supply Warning Set Threshold info icon to view the tooltip message.

C-Bus Power Supply Warning Clear Threshold

  • By default, Disabled is selected.

  • The value selected must be less than the C-Bus Power Supply Warning Set Thresholdvalue selected.

  • If the C-Bus Power Supply Warning Set Threshold is Disabled, then setting a value here will also set the C-Bus Power Supply Warning Set Threshold value to (current C-Bus Power Supply Warning Clear Threshold value + 10 mA).

Mouse over on the C-Bus Power Supply Warning Clear Threshold info icon to view the tooltip message.

Unit Over Temperature Set Threshold

This field is a combo box which is by default set to 70° C.

The Unit Over Temperature Set Thresholdproperty increments by 1° C with a range of 1° C - 80° C.

Mouse over on the Unit Over Temperature Set Threshold info icon to view the tooltip message.

Unit Over Temperature Clear Threshold

This field is a combo box which is by default set to 65° C.

The Unit Over Temperature Clear Threshold property increments by 1° C with a range of 0° C - 79° C.

Mouse over on the Unit Over Temperature Clear Threshold info icon to view the tooltip message.

Measurement

Device ID

This field displays the unit address of the device.

NOTE: The Device ID is for the entire device and is as same for Error Reporting section.

When you assign a Device ID, and if you set the Device ID to Not Assigned, then all properties in both the Error Reporting and Measurement section are reverted to their default settings and disabled (grey out state).

Send Trigger Group

This field contains a trigger group to request the relays to send its stored measurement data.

Mouse over on the Send Trigger Group info icon to view the tooltip message.

Clear Trigger Group

This field contains a trigger group to clear the stored measurement data in the relays.

Mouse over on the Clear Trigger Group info icon to view the tooltip message.

Regular Broadcast Interval

NA

Disabled by default. Can set the intervals between 1 min to 4 hours.

Regular Broadcast Option

All

Enabled by default.

Lamp Hours

Selected and disabled by default.

Channel Temperature

Selected and disabled by default.

Power Supply Current

Selected and disabled by default.

C-Bus Voltage

Selected and disabled by default.

Unit temperature

Selected and disabled by default.

NOTE: Deselecting all will enable each of the individual check box options.
Destination Network

This field contains the destination C-Bus network to which the relays routes measurement application messages.

Mouse over on the Destination Network info icon to view the tooltip message.

The action selector for trigger groups is as explained below:

Virtual Channel Number

Property

Units

Reset

Notes

0 – 15

Lamp Running Time

Hours

Yes

NA

16 – 31

Channel Voltage

Volts

No

Units with power metering only

32 – 47

Channel Current

Amperes

No

48 – 63

Channel Power

Watts

No

64 – 79

Channel Energy

Watt-hours

Yes

80 – 95

Channel Lifetime Energy

Watt-hours

No

128 – 143

Channel Temperature

Celsius

No

relays only

252

C-Bus Power Supply Output Current

Amperes

No

NA

253

C-Bus Voltage

Volts

No

NA

254

Unit Temperature

Celsius

NA

NA

Measurement Application supports various operational parameters for triggered request.

Measurement Request Trigger Group defines the Trigger Group for the request. A trigger's Action Selector determines which measured parameter is requested.

NOTE: Action Selector 0xFF requests all measurements (in which they are sent 2 at a time with an interval of 2 seconds). Other Action Selector values can be used to request individual measured properties corresponding to the virtual channel number as per the above table.

The DEVICE ID for the Measurements is defined by the Device ID parameter, the same Device ID is used for Error Reporting. The Device ID will be unique per network to differentiate measurements from different devices. The devices monitoring the Measurement messages should keep track of the source network to differentiate if Device IDs are reused across multiple C-Bus networks.

If the Device ID parameter is left at its default value of 0xFF then the Unit Address is used as the Device ID in the Measurement Application messages, which ensures uniqueness. However, if the device is readdressed then any monitoring devices will also needs to be updated to match the new Device ID (It is recommended to leave the Device ID as the default value).

Logic Groups

relays can have maximum 4 logic groups each group having respective channels (8 or 4)

Group

This section will allow to create a enable group using and modify existing group using .

By default, it is unused. If enable group is created, Restore To Previous is enabled.

Power Recovery

This field allows to set the power recovery percentage. By default, it is Restore to Previous.

Channel

NOTE :

  • RELDN16A will have 16 channels

  • RELDN8A will have 8 channels

  • RELDN4A will have 4 channels

Global

This section displays the project properties set by the user at the time of creation of the project.

C-Bus Clock

If checked, allows you to enable the C-Bus clock for the relays.

Disable Local Toggle

If checked, disables the local toggle.

Disable Power Supply Toggle

If checked, disables the power supply toggle.

Disable C-Bus Priority

If checked, disables the C-Bus priority.

Disable Clock Generator Toggle

If checked, disables the clock generator toggle.

Unit Identification

This section display the fields for identification of the unit.

Unit Type

This field contains the unit type and unit description of the device.

Catalog Number

This field contains the catalog number related to the unit type.

Firmware Version

This field shows the version number of the C-Bus interface firmware which exists on the physical network or which has been assigned to a logical representation of the unit in the database.

Part Name

This field contains the part name which is stored in the unit hardware, which can be modified.

Unit Address

This field displays the unit address assigned to the device.

Serial Number

This field contains the serial number which exists on the physical network.

Tag Name

This field contains the name that user can give to the logical representation of the unit. This name can be up to 32 characters long and is stored in the project database only.

Notes

This field contains a location to add notes about the unit which is stored in the project database only.

Status

The Status section contains information about the C-Bus network related functions located on the unit.

Device Status

This section displays the details of hardware.

Hardware Version

This field displays the hardware version of the device.

Firmware Version

This field displays the firmware version of the device.

C-Bus Clock Active

This field indicates whether the C-Bus internal clock is currently enabled on the relays within the network.

C-Bus Voltage (V)

This field displays the C-Bus voltage of the device.

Inbuilt C-Bus Power Supply Active

This field displays whether the Inbuilt C-Bus Power Supply Active is On or Off.

Power Supply Load

This field displays the load of the power supply (mA).

Power Supply Output Voltage

This field displays the power supply output voltage (mV) of the device.

Load Power

This field displays the load power (mW) of the device.

Unit Temperature

This field displays the unit temperature (°C) of the device.

Once configuring relay is completed, click Save to save the changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?