Software Version 2.14.0

Input Unit

The input units allow users to interact with the system or get input from the environment by means of sensing devices.

  • Wall switches have input keys which allow users to utilize short press/release and long press/release actions to affect lighting control.

  • Sensors, on the other hand, are units which convert data from sensing devices into C-Bus messages.

  • General input units receive analog or digital measurements from channels and convert the signals into event and broadcast measurement messages via the C-Bus.

Input units can be used to:

  • Control lighting conditions by manual switching or as a response to changes in lighting levels.

  • Control air conditioning according to ambient temperature.

  • Control security and access systems by responding to human presence or predetermined codes.

  • Convert measurement data into C-Bus event messaging.

C-Bus input units respond to certain stimuli - human touch, ambient light conditions, temperature and infrared radiation - and then send messages to appropriate output units in a predetermined way.

The devices under Input unit category are as listed below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.