Software Version 2.14.0

Library Window

The Library window lists the C-Bus Unit and DALI devices available for use in the project. The relevant device types are displayed with respect to whether a C-Bus network or DALI gateway is selected in the Explorer window. The operations are performed with regards to a C-Bus device or a DALI device added in the network of the SpaceLogic C-Bus Commission software.

The different operations performed in Library window are:

Search a Device

Prerequisites: A project must already be open in the Explorer window with a network created in the project.

The Library window allows searching for a device. The device appears on the list, after the name of the device is entered in the search bar.

  1. Select a network in the Explorer window

  2. In the Library window, enter the name of the device in the search bar

    Step result: Related devices are displayed in the Library window.

    TIP: The device can be searched either by giving catalogue number, unit type or category.

Filter

The displays the devices in the Library window based on the categories.

To remove the applied filter, Click and click Clear All

Unit Type Categories

C-Bus units can be divided into categories according to their functional role. The general categories are listed below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.