Software Version 2.14.0

Edit Enable Group

Prerequisites: Make sure you have selected Enable application and enable groups has been created.
  1. Double-click on the enable group name that has to be edited/renamed
    Step result: Edit Enable Group Dialog box is displayed.
  2. Edit the Enable Group name and click OK
    NOTE: Special characters except / , “,# and maximum of 32 characters in the Enable group name are valid.
    Step result: The Enable group name is updated.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.