Software Version 2.14.0

Application Log

Prerequisites: The network must already be created.

Application Log displays the communications performed in an open network. This window also allows searching for a device, by entering the device name, part number or description fully or partly in the search bar.

When a network is being used, applications and their devices generate log events which are displayed in the Application Log.

Fields

Description

Date & Time

This field refers to the date and time for the log entry.

Application

This field refers to the application type of the log.

Group

This field specifies the address of the application group that has generated the log entry.

Device

This field provides information about the unit that issued the message.

Event

This field provides information about the status or event which the entry is logging. The event information varies with the type of application.

Operation performed on application log:

  • Search Bar- Keyword search for the existing log entries..

  • - Filter by application, group and device addresses.

  • - Save the application log.

  • - Pause/Play the application log.

  • - Erase the application log events.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.