Software Version 2.14.0

Add Test Devices

The Devices section allows to add test devices which further is assigned to particular test groups created.

  1. In Devices section, click

  2. A pop-up is displayed

    • Select the CDG address (0–254)

    • Define the CDG name, or use the default name

    • Select the DALI line (A/B)

    • Define the Line name, or use the default name

    • Type the number of multiple object ID’s to be added (maximum 64 can be added at a time)

    • Select the start of Object ID

    • Define the EEL name, or use the default name

    • Select the Light Source Life value (400 - 7300) in days

      NOTE: Value can be modified once the device is added.
    • Assign the test group for the device

      NOTE: By default, it will be unassigned and can be modified once the device is added.

Click Add Devices

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.