Software Version 2.14.0

Measurement Application

Prerequisites: The network must have already been created in the project .

The Measurement application receives raw data in the form of voltage, current and resistance. This information is converted, scaled and then transmitted across the C-Bus to accurately represent physical measurement units such as temperature, liquid level, light level, etc. The measurement data transmitted across the C-Bus is utilized by C-Bus unit such as temperature, liquid level, light level, etc., which can process measurement application messages.

Measurement application is created using a reserved application address 228.

SpaceLogic C-Bus units which support measurement application.

  • General input unit

  • current measurement unit

  • 5104DTSI temperature sensor

  • Color C-Touch Screen

  • PAC module

  • Schedule Plus +

  • HomeGate

  • eDLT key input unit

  • DALI Gateway

  • 8 Channel Switchable Power Supply Dimmer

  • 4 Channel Switchable Power Supply Dimmer

  • DALI-2 Gateway

The procedure to create an measurement application is similar to creating error application with a reserved address 228.

The field informations of measurement application is as explained below:

Field

Meaning

Device ID

Unique Device ID is a reference to identify a specific C-Bus unit for measurement report. The measurement Device ID drop down list allows the ability to select a value from 0- 254.

Device Name

The Device name specifies the name of the device. The drop-down list allows the selection of a unique ID between 1 - 254.

Channel ID

The Channel ID is used to specify the channel of the device from which the Measurement application data is received. The channel ID drop-down list allows the ability to select a value from 0- 255.

NOTE: Channel ID starts at the next available address based on the device ID.

Channel name

The Channel name specifies the name of the channel.

Timeout Period

Time out value that is used by the Controller to monitor the object (0–2880 minutes).

  • If no timeout value is added, it is considered as invalid with blank.

  • If the timeout is 0, then the value are read and updated normally.

Unit Type

The Unit type displays the unit type of the value read. The below table explains the standard units that are used in measurement application.

Current Value

The Current value displays the current read value.

Standard Measurement Units

The table below contains a list of measurement units which are available to select when converting input data into measurement data for transmission across the C-Bus system.

Unit Code

Units

Typical Use

$00

°C

Temperature

$01

Amps

Current

$02

Angle (degrees)

Angular displacement

$03

Coulomb

(Electric charge)

$04

False=0

 

True otherwise

Boolean stuff

$05

Farads

Capacitance

$06

Henrys

Inductance

$07

Hertz

Frequency

$08

Joules

Energy

$09

Katal

Rate of catalytic activity

$0A

Kg/m3

Density

$0B

Kilograms

Mass

$0C

Liters

Volume

$0D

Liters per hour

Very slow flow rate

$0E

Liters per minute

Slow flow rate

$0F

Liters per second

Flow rate

$10

Lux

Light Level

$11

Metres

Distance

$12

Metres per minute

Slow speed

$13

Metres per second

Speed

$14

Metres/s2

Acceleration

$15

Mole

Quantity of substance

$16

Newton metre

Torque

$17

Newtons

Force

$18

Ohms

Resistance

$19

Pascal

Pressure

Operations performed in Measurement application

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.