Software Version 2.12.0

Sort Test Groups

Prerequisites: The Test Group Addresses must already been created in the Emergency Exit Light application.

The existing test groups in application can be sorted.

  1. Select the Test Group.

    NOTE:
    • A single test group can be chosen by selecting the check box of the required group, whereas all test groups can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one test group, then hold down the SHIFT key and select on additional test group (grid) using the mouse.

    • For random multiple selection, select one test group, then hold down the CTRL key and select the next test group (grid) using the mouse.

  2. Click in the Test Groups section.

    The available sort methods are displayed.

  3. Select the appropriate sort method. The Test Group list will be sorted according to the selected sort method.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?