Software Version 2.14.0

Knowing the User Interface

Outline

The home screen of SpaceLogic C-Bus Commission Software after the installation is as below:

Customizing the User Interface Layout

You can customize the appearance of the commission software User Interface by modifying the layout of windows . You can modify their size and also their position.

  • Windows can be arranged:

    • Pinned

    • Docked

    • Floating on multiple monitors

The customized layout is saved when you close the commission software.

TIP: To get the default setting, see Reset window layout

The following demonstrates an example of a customized User Interface layout.

Each Window consists of following control buttons:

Button

Description

Drop-down options

  • Float

  • Dock

  • Dock as document

  • Auto hide

  • Close

Auto hide

Close the window

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.