Software Version 2.14.0

Workspace Window

The Workspace window displays the devices in the project and the network. This window allows you to connect your project's devices to the network.

This window consists of two built-in sections for C-Bus Devices:

  1. Devices in Project

  2. Network Devices

For Dali Devices

Prerequisites: The DALI-2 Gateway must be already added.

This window consists of two built-in sections for Dali Devices:

  1. (DALI) Devices in project

  2. Line devices

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.