Software Version 2.14.0

DALI ECG Devices

This section allows the user to configure different operational features for devices in the DALI line added to each network.

Unit Types

  • DALI ECG DT1 (Emergency or Exit Light (Generic))

  • DALI ECG DT1 A (Emergency or Exit Light (Switched Maintained Dimmable))

  • DALI ECG DT1 B (Emergency or Exit Light (Switched Maintained Non-Dimmable))

  • DALI ECG DT1 C (Emergency or Exit Light (Maintained))

  • DALI ECG DT1 D (Emergency or Exit Light (Non – Maintained Dimmable))

  • DALI ECG DT 6 (Single Channel LED Device)

  • DALI 2x ECG DT 6 (DALI 2 Channel Device (DT6))

  • DALI 3x ECG DT 6 (DALI 3 Channel Device (DT6))

  • DALI 4x ECG DT 6 (DALI 4 Channel Device (DT6))

  • DALI ECG (DALI ECG (Generic))

  • DALI 2x ECG (DALI 2 Channel Device (Generic))

  • DALI 3x ECG (DALI 3 Channel Device (Generic))

  • DALI 4x ECG (DALI 4 Channel Device (Generic))

  • DALI ECG DT8 (Single Channel Tunable / Color Controllable Device))

The field information to configure DALI ECG devices is as explained below:

Channel Info

Name

This field allows to modify the DALI Channel name.

Description

This field allows to give description on channel device.

 

Applications

This section displays the lighting applications supported by the DALI-2 Gateway. Up to four lighting applications can be defined and then used throughout the configuration of the DALI-2 Gateway.

Control Mapping

Device Used

This field lets you know whether the device is physically available or not.

By default, the check box is checked.

Address Mapping

Address Mapping allows a C-Bus group address to directly control a DALI device.

It is a one to one mapping of a C-Bus group address to a DALI device.

NOTE: Only controllable DALI devices support Address Mapping.

This section allows to assign maximum of 16 DALI group membership.

NOTE: If the check box is selected, then the group is used for the device.

Brightness Group

C-Bus group address is mapped to control the Address Mapping.

IMPORTANT: The groups assigned in Line A, Line B, and DALI devices on each line has to be unique.

CCT/Hue Group

C-Bus group address is used to control the CCT/Hue of a DALI DT8 device.

  • If a Saturation Group is not set, this CCT/Hue Group controls the CCT (correlated colour temperature).

    Used in conjunction with the Brightness Group for on, off, and dimming control plus setting the white colour temperature (tuneable white).

  • If a Saturation Group is set, this CCT/Hue Group controls the Hue of a DALI DT8 device.

NOTE:
  • The CCT/Hue Group uses the Application Index defined in the Brightness Group.

  • The CCT/Hue Group is applicable to all controllable DALI devices (excluding Emergency Types C and D), yet functional for DALI DT8 only.

Saturation Group

C-Bus Group Address is used to control the Saturation of a DALI DT8 device.

  • If a CCT/Hue Group is set, this CCT/Hue Group controls the Hue (colour) of a DALI DT8 device.

    The Saturation Group controls the Saturation (intensity) of a DALI DT8 device.

  • Used with both the Brightness Group and the CCT/Hue Group for on, off, and dimming control plus setting the RGB colour and its intensity.

NOTE:
  • The Saturation Group uses the Application Index defined in the Brightness Group.

  • The CCT/Hue Group is applicable to all controllable DALI devices (excluding Emergency Types C and D), yet functional for DALI DT8 only.

Disable DALI to C-Bus Mapping

Check the checkbox to disable the DALI to C-Bus mapping

Application Index

This field is a combo box to select the application to be used for the group.

The index is visible only when the application is been assigned in the application section.

Warn Before Off Time

This field displays the amount of time after the group address is turned off (1–15 minutes).

Advanced

Min Max Logic

This field gives the ability to pair 2 C-Bus group address to the same logical output and perform minimum and maximum logic.

Logic group Assignment

This field allows you to pair additional groups to the output.

Virtual Groups

This section refers to a category for virtual groups, which is an extension of DALI groups and allows to create a maximum of 16 Virtual groups.

Device Control

Levels

Minimum Level

This field displays the minimum level for the device. This value cannot be lower than the Physical Minimum Level.

Maximum Level

This field displays the maximum level for the device.

Power On Level

This field displays the level that the device will reach when it powers on from an off state.

System Failure Level

This field allows to set system failure level.

Physical Minimum Level

This field displays the physical minimum level, which is defined by the manufacturer.

Emergency Level

This field displays the emergency level for the device if it was a DALI emergency and exit ECG. The device will reach this level when the mains power is out and the device is running on battery.

Prolong Time

This field displays the prolong time for this device.

Test Timeout

This field displays the test timeout for the device. This refers to the count of how many times the device times outs before it stops the test.

Physical Minimum Level

This is a read only field. This refers to the device physical minimum level.

Emergency Minimum Level

This field displays the minimum level the DALI emergency and exit ECGs will reach. This field is for DALI emergency and exit ECGs only.

Emergency Maximum Level

This field displays the maximum level the DALI emergency and exit ECGs will reach. This field is for DALI emergency and exit ECGs only.

Rated Duration

This field displays the rate duration for the device.

Lamp Time

This field displays the lamp running time. This is only updated when the device is extracted.

Remote On

This field is used to enable or disable Remote ON. If selected, the Remote ON is enabled. If cleared, the Remote ON is disabled.

Remote Off

This field is used to enable or disable Remote OFF. If selected, the Remote OFF is enabled. If cleared, the Remote OFF is disabled.

Scenes

NOTE: The user must have configured the scene configuration in the DALI Gateway lines.

This is the category section for scenes, where a user is allowed to assign maximum 16 DALI scenes to each controllable devices.

By assigning the scene, the user can set the level they want the scene to go to based on min and max level of the device.

Minimum Level – minimum level the device has been set to.

Maximum Level – maximum level the device has been set to.

Led Light

This is the category section for the dimming curve type.

Dimming Curve Type

This field displays the dimming curve type set for the DT6 device. This can be either standard dimming curve or linear dimming curve.

Emergency Light

Status

Inhibit Mode

If checked, notifies when the device is in preventing mode.

Function Test Done and Result Valid

If checked, notifies when the function test is completed and is valid.

Duration Test Done Result Valid

If checked, notifies when the duration test is completed and is valid.

Battery Fully Charged

If checked, notifies when the battery is fully charged.

Function Test Request Pending

If checked, notifies when the function test request is pending.

Duration Test Request Pending

If checked, notifies when the duration test request is pending.

Identification Active

If checked, notifies when the device is identified (50/50, identify).

Physically Selected

If checked, notifies if this device is the one physically selected.

Mode

Rest Mode Active

If checked, will be in currently off mode.

Normal Mode Active

If checked, will be in normal on mode.

Emergency Mode Active

If checked, will be in emergency mode.

Extended Emergency Mode

If checked, notifies when the extended emergency mode is in use.

Function Test in Progress

If checked, notifies when the function test is in progress.

Duration Test in Progress

If checked, notifies when the duration test is in progress.

Hardwired Inhibit is Active

If checked, notifies when the hardwired inhibit is active.

Failure Status

Circuit Failure

If checked, notifies when there is circuit failure.

Battery Duration Failure

If checked, notifies when there is battery duration failure.

Battery Failure

If checked, notifies when there is battery failure.

Emergency Lamp Failure

If checked, notifies when there is emergency lamp failure.

Function Test Max Delay Exceeded

If checked, notifies when the function test max delay is exceeded.

Duration Test Max Delay Exceeded

If checked, notifies when the duration test max delay is exceeded.

Function Test Failed

If checked, notifies when the function test max delay is exceeded.

Duration Test Failed

If checked, notifies when the duration test is failed.

Features

This section displays the parameters whose values get reported from the emergency application.

Integral Emergency Control

If checked, the parameter value gets reported.

Maintained Control Gear

If checked, the parameter value gets reported.

Switched Maintained Control Gear

If checked, the parameter value gets reported.

Auto Test Capability

If checked, the parameter value gets reported.

Adjustable Emergency Level

If checked, the parameter value gets reported.

Hardwired Inhibit Supported

If checked, the parameter value gets reported.

Physical Selection Supported

If checked, the parameter value gets reported.

Relight in Rest Mode Supported

If checked, the parameter value gets reported.

Light Source Life

This field displays how long the device is been running for (in hours).

Battery Charge Percent

This field displays the percentage of the battery on the current amount of time.

Duration Test Result Minutes

This field displays how long the device has run duration test result.

Lamp Emergency Time

This field displays how long the device has run its emergency mode.

Lamp Total time

This field displays normal operation time along with emergency time.

Status

This section is read-only. This will update only when extracted from the device

Control Gear Failure

If checked, notifies when there is a control gear failure.

Lamp Failure

If checked, notifies when there is a Lamp failure.

Lamp On

If checked, notifies when there is a Lamp On.

Limit error

If checked, notifies when there is a Limit error.

Fade Running

If checked, notifies when there is a Fade running.

Reset state

If checked, notifies when there is a Fade running.

Short Address Missing

If checked, notifies when the short address is missing.

Power Cycle Seen

If checked, notifies when the power cycle is seen (when the device is turned off and back on again).

Thermal Overload Detected

If checked, notifies when the thermal overload is detected.

Thermal Shutdown Detected

If checked, notifies when the thermal shutdown is detected.

Load Decreased Detected

If checked, notifies when the load decrease is detected.

Reference Measurement Failed

If checked, notifies when the reference measurement is failed.

Load Increased Detected

If checked, notifies when there is a Fade running.

Reconciled

If checked, notifies the device has been reconciled. If not checked, the device is not reconciled.

Device Identification

Short Address

This field displays the short address of the device.

Object ID

This field displays the object ID of the device.

GTIN

This field displays the GTIN number of the device and is updated only after the device is extracted.

Serial

This field displays the device’s serial number and is updated only after the device is extracted.

Device Type 0

If selected, then the device is type 0. If cleared, then the device is not type 0.

Device Type 1

If selected, then the device is type 1. If cleared, then the device is not type 1.

Device Type 6

If selected, then the device is type 6. If cleared, then the device is not type 6.

Device Type 8

If selected, then the device is type 8. If cleared, then the device is not type 8.

DALI Version

This refers to the DALI version of the device and is updated after the device is extracted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.