Software Version 2.14.0

Properties Window

This window displays C-Bus and DALI device properties where the name and type of the device can be updated. This also allows the user to configure different operational features for C-Bus and DALI devices added to each network.

TIP: The properties of any units can also be loaded using Load Properties in Network Device/Line Device (for DALI devices) section of WORKSPACE window.

To View/Edit C-Bus Device Properties

Prerequisites:

  • A project must be open in the SpaceLogic C-Bus Commission software. The C-Bus devices must already be added to a Devices in Project of a network.

  • This section displays the name and type of the C-Bus device. The name of the C-Bus device can be renamed and also allows you to configure different operational features for C-Bus devices added to each network.

  1. Select a Network from the project.

  2. Click C-Bus Devices of a network.

  3. Select a C-Bus unit device from Devices in Project.

    Step result: The selected C-Bus device properties are displayed in the PROPERTIES window.

    NOTE: The fields in the device properties can be modified as per the project requirement.

To View/Edit DALI Device Properties

Prerequisites:

  • A project must be open in the SpaceLogic C-Bus Commission software. The DALI gateway and DALI device must already be added to a Devices in Project of a network (Adding DALI Gateway is similar to adding any C-Bus device).

  • This section displays the name and type of the DALI device. The name of the DALI device can be renamed and also allows the user to configure different operational features for DALI devices added to a DALI line in each network.

  1. Click DALI devices drop-down in the EXPLORER window.

    NOTE: DALI devices are visible only when DALI Gateway is added from LIBRARY window to Devices in Project of WORKSPACE window.

  2. Choose a DALI line.

  3. Select a DALI device from Devices in Project from WORKSPACE window.

    Step result: The selected C-Bus device properties are displayed in the PROPERTIES window.

NOTE: The fields in the device properties can be modified as per the project requirement.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.