Software Version 2.14.0

Relays

C-Bus relay units are output devices used to switch resistive, fluorescent and inductive loads. The relay units are available with switched active outputs and voltage free variants, mechanically latching relay outputs on specific C-Bus relays.

SpaceLogic C-Bus provides a range of relays.

  • Voltage Free Relays

To configure Voltage free relays, click here

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.