Software Version 2.14.0

Groups

A Group Address is used to make associations between the key of an Input Unit and the channel of an Output Unit. They are assigned to output and input units to commission the devices for controlling the same object.

NOTE:
  • A number of C-Bus Output Unit channels can be controlled by a single key on a C-Bus switch (with the same Group Address).

  • A number of keys on different Input Units can control the same load, by giving them all the same Group Address.

There are 255 Group Addresses (0 to 254) in an Application Address. SpaceLogic C-Bus allows the creation up to 255 different Group Addresses on each Application Address.

Operations performed on groups:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.