Software Version 2.14.0

Paste Group

Prerequisites: The Group Address must be copied from an application to another network or to the same network.

The application Group Addresses copied from one network can be pasted to an another application in different network. The complete application copied from one network can also be pasted to an another network.

NOTE: The lighting application Group Address copied from one network can be pasted into the lighting application on another network only.
  1. Open the Groups section of Lighting application.
    NOTE: Paste the Group Address in lighting application of an another network.
  2. Click in the Group section of a lighting application.
    NOTE: The process to Paste the Group Address from excel is as demonstrated below:
IMPORTANT: Paste conflict occurs when already existing group name and group address are been pasted.

The process to Resolve conflict is as demonstrated below:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.