Software Version 2.14.0

Paste Action Selectors

The paste option allows the user to paste the Action Selectors copied from one Trigger group into a different Trigger group on the same network or into a Trigger Group on another network, or in another project.
Prerequisites: The Action selectors must already be copied from a Trigger Group.
  1. Select a trigger group in Trigger groups section.
    NOTE: Action selectors can either be pasted on same network or into a Trigger Group on another network/project.
  2. Click in the Action selectors section.
    NOTE: The Process to Paste Action selectors from Excel is similar to as demonstrated in lighting application, click here
    Step result: The copied Action selectors are pasted.
IMPORTANT: Paste conflict occurs when already existing Action selector name and Action selector address are been pasted in Trigger application.

The process to Resolve conflict is similar to as demonstrated in lighting application, click here

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.