Software Version 2.14.0

Delete Media Link Groups

Prerequisites: Media Transport application must already be created in the network and Media Link Groups must be added.
  1. Select Media Link Group.

    NOTE:
    • A single Media Link Group can be chosen by selecting the check box of the required group, whereas all Media Link Group can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one Media Link Group, then hold down the SHIFT key and select on additional Media Link Groups (grid) using the mouse.

    • For random multiple selection, select one Media Link Group, then hold down the CTRL key and select the next Media Link Group (grid) using the mouse.

  2. Click in the Media Link Group section. A Confirmation pop-up is displayed.

  3. Click Yes to delete the Media Link Groups and No to cancel the delete operation.
    TIP: Alternate method to delete selected Media Link Group is, right-click on selected media link group > Delete.

Repeat the steps 1–3 for deleting levels.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.