Software Version 2.14.0

Add Media Link Groups

Prerequisites: The Media Transport application must already be created in a network.

Media Transport application allows to create a maximum number of 255 media link groups.

  1. Click Applications drop-down in the Explorer window.
  2. Click Media Transport.
  3. Click

    Step result: A individual media link group is added.

    The media link group table:

    • displays the total number of media link groups created.

    • can have maximum of 255 media link groups.

    • by default, the media link group name is ‘Media Link Group X’ (‘X’ is the number of the media link group).

    • cannot add multiple media link groups at a time.

    IMPORTANT:
    • A media link group can be deleted during creation/adding itself using “x” as shown below:

  4. The media link group name can be modified. Double-click on the media link group name, edit the media link group name and click enter (or on the empty space of the section) to update the change.
Along with the media link group section, the media transport application workspace consists of functions of each selected media link group and the respective levels of the media link group function.

The levels for the media link group functions are as below

NOTE: The levels for function are applicable only for below media link group functions.

Functions

Level

Name

Play/Stop

0

Stop

1

Play

Pause/Resume

0

Pause

255

Resume

Shuffle

0

Shuffle off

255

Shuffle on

Repeat

0

Repeat off

1

Repeat current

255

Repeat all

Forward

and

Rewind

0

Normal speed

2

2x speed

4

4x speed

6

8x speed

8

16x speed

10

32x speed

12

64x speed

Source Power Control

0

Source power off

255

Source power on

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.