Software Version 2.14.0

Devices

Devices section allows to assign devices for particular test group created.

The field information of the device section are as explained below:

Fields

Meaning

CDG Address

Displays the C-Bus DALI-2 Gateway Address

CDG Name

Displays the C-Bus DALI-2 Gateway name

Line A/B

Displays the selected line for device

Line Name

Displays the line name

Object ID

Displays the Object ID of the device

EEL Name

Displays Emergency Exit Light name

Light Source Life

Displays how long the device is been running for (in days)

Test Group

Displays the assigned test group

NOTE:
  • The devices created must match the Emergency and Exit device details on the target DALI-2 Gateway on the network

  • All assigned devices to the deleted test group will be unassigned

Operations performed on Devices section are:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.