Software Version 2.14.0

Wall Plates/Key Input Unit

SpaceLogic C-Bus provides a range of Key Input units.

  • Saturn

  • Saturn Zen

To upgrade Wall Plates/Key Input Unit firmware, Unit firmware updater.

Unit Types

Category

Catalog Number

Unit Type

Description

Saturn

‘A’ Series

5082680

KEYB2A

2 Gang Saturn Key Input Unit

5082GF

5082J80

5082PW

5084680

KEYB4A

4 Gang Saturn Key Input Unit

5084GF

5084J80

5084PW

5086680

KEYB6A

6 Gang Saturn Key Input Unit

5086GF

5086J80

5086PW

‘E’ Series

E5082680

KEYB2A

2 Gang Saturn Key Input Unit

E5082GF

E5082PW

E5084680

KEYB4A

4 Gang Saturn Key Input Unit

E5084GF

E5084PW

E5086680

KEYB6A

6 Gang Saturn Key Input Unit

E5086GF

E5086PW

Saturn Zen

‘A’ Series

R5041ZB

KEYH1A

1 Gang Saturn Zen Key Input Unit

R5041ZW

R5042ZB

KEYH2A

2 Gang Saturn Zen Key Input Unit

R5042ZW

R5043ZB

KEYH3A

3 Gang Saturn Zen Key Input Unit

R5043ZW

R5044ZB

KEYH4A

4 Gang Saturn Zen Key Input Unit

R5044ZW

‘E’ Series

ER5041ZB

KEYH1A

1 Gang Saturn Zen Key Input Unit

ER5041ZW

ER5042ZB

KEYH2A

2 Gang Saturn Zen Key Input Unit

ER5042ZW

ER5043ZB

KEYH3A

3 Gang Saturn Zen Key Input Unit

ER5043ZW

ER5044ZB

KEYH4A

4 Gang Saturn Zen Key Input Unit

ER5044ZW

To Upgrade Key Input Unit firmware, click here.

The field informations to configure SpaceLogic C-Bus Saturn and Saturn Zen series are described as below:

Applications

This section displays the lighting applications supported by the Saturn and Saturn Zen series. Up to four lighting applications can be defined and then used throughout the configuration of the Saturn and Saturn Zen series each.

Keys

Depending on the input unit selected, the number of keys will vary

Profiles Enable Group

Allows to create a new enable group.

By default, <unused> is selected.

Click to create a new enable group.

Click OK once the profiles are edited.

Profiles Enable Group

By default, <unused> enable group is selected.

Click to edit the enable group name.

Click to create a new enable group.

Profiles Selection

Once the enable group is selected, one or all profile can be selected (profile 2, profile 3, profile 4).

Profile 1 is selected by default and remains along with other profile selection.

Disable All Keys

Select the check box to disable all the keys.

No key functions will be working if set.

Profile Name

Profile 1 is selected by default along with the chosen profiles.

To edit the profile name, select the profile name and type the new one.

Power Recovery

By default, profile 1 name will be selected.

Profile

Allows the keys to change their behavior when triggered. Up to four profiles can be used.

Profiles utilize different widgets to define alternate (or same) key behavior for each profile.

All the profiles will be available. By default, profile 1 will be selected.

Key

Each keys can have max of 16 widgets created in it.

Widget

Displays the selected widget and application for a particular key.

Depending on the application chosen the key property differs.

  • Widget: Can choose widgets ranging from 1–16.

  • Click drop-down next to the widget to select the application.

  • Click to add new widget.

  • Click to remove the widget.

Function

Click here for more details.

Group

Select any existing group or create new using , or edit group name using .

Across all widgets in a group, the group address remains the same.

Ramp Rate

Ramp rate can be set from instant to max 17 minutes.

Indicator

Indicator Assignment

Any of the 16 widget can be assigned to the indicator.

Indicator On Color

Indicator color can be set to:

  • Off

  • 8 different colors

  • 2 User-defined

  • Dynamic (using C-Bus group to control)

NOTE: is enabled only for user defined and dynamic changes.

Indicator Off Color

Indicator color can be set to:

  • Off

  • 8 different colors

  • 2 User-defined

  • 5 Dynamic (using C-Bus group to control)

NOTE: is enabled only for user defined and dynamic changes.

The table below explains the details of widgets selected with its functions.

Lighting

Function

Allows to select different function available for selected application.

Select one of the below lighting functions:

  • Toggle

  • On

  • Off

  • Preset

  • Toggle Dimmer

  • Toggle Dimmer Down

  • Toggle Dimmer Up

  • Memory Toggle Dimmer

  • Memory Toggle Dimmer Down

  • Memory Toggle Dimmer Up

  • Dimmer Down

  • Dimmer Up

  • Down

  • Up

  • Soft Down

  • Soft Up

  • Nudge Down

  • Nudge Up

  • Bell Press

  • Custom 1

  • Custom 2

  • Custom 3

  • Custom 4

If custom function is selected, files can be imported and exported to software using and respectively.

Group

Select any existing group or create new using ,or edit group name using .

Across all widgets in a group, the group address remains the same.

Ramp Rate

Ramp rate can be set from instant to max 17 minutes.

Restore Level

By default, restore level is set to 0%.

Timer

Function

Allows to select different function available for selected application.

Select one of the below timer functions:

  • Retrigger Timer

  • Toggle Timer

  • Delay Timer

  • Pulse Timer

Timer Level

Allows to adjust timer level to a max of 100% (255) to min of 1% (1).

Ramp Rate

Allows to set ramp rate between 4 sec to 17min.

Duration

Set the duration for the timer.

Expiry Level

By default, set to 0%. Expiry level value varies from 0 - 100%.

Expiry Ramp Rate

By default, expiry ramp rate is set to instant. The values vary from 4 seconds to 17 minutes.

Enable Timer Flash

Select the check box to enable indicator status. By default, it is enabled.

Restore Level

Assigned restore level is common across widgets with the same group which varies from 0 to 100%.

Shutter Relay

One of the following shutter relay functions can be selected:

  • Shutter Toggle

  • Shutter Open/Stop

  • Shutter Close/Stop

  • Shutter Open

  • Shutter Close

  • Shutter Stop

Enable

One of the following enable functions can be selected:

  • Unused (Default)

  • Toggle

  • On

  • Off

  • Preset

    • Preset Level:

      Allows to set the preset level between 0 - 100 %

Enable Group

Select any existing group or create new using , or edit group name using .

Restore Level

Assigned restore level is common across widgets with the same group which varies from 0 to 100%.

Fan Cycle

Trigger Group

Select any existing group or create new using , or edit group name using .

Action Selector

Select any existing action selector or create new using , or edit action selector name using .

Scene

One of the following scene functions can be selected:

  • Scene Toggle (Default)

  • Scene Set

  • Scene Off

  • Scene Off/Down

  • Scene On/Up

Scene Label

Select the scenes between 1 - 8.

Click for scene manager.

Ramp Rate

Allows to set ramp rate between 4 sec to 17min.

This parameter is applicable only for scene functions Scene Off/Down and Scene On/Up.

Trigger Group

Select any existing group or create new using , or edit group name using .

Action Selector

Select any existing action selector or create new using ,or edit action selector name using .

Enable Scene Repair

Enable the scene repair by checking the check box.

Enabling the scene repair will maintain the scene status if all the items in the scene, match the current live state.

Sequence

One of the following scene functions can be selected:

  • Sequence Toggle (Default)

  • Sequence Start

  • Sequence Off

  • Sequence Reverse Toggle

  • Sequence Reverse Off

  • Sequence Stop

Sequence Label

Select the sequence between 1 - 8.

Click for sequence manager.

Trigger Group

Select any existing group or create new using , or edit group name using .

Action Selector

Select any existing action selector or create new using , or edit action selector name using .

Use Delay For Off

Check the check box to enable delay off.

Audio

Function

Allows to select different function available for selected application.

Select one of the below audio functions:

  • Volume Up

  • Volume Down

  • Volume Cycle

  • Treble Up

  • Treble Down

  • Treble Cycle

  • Bass Up

  • Bass Down

  • Bass Cycle

  • Balance Left

  • Balance Right

  • Balance Cycle

  • Next Source

  • Previous Source

  • Preset Source

  • Dynamic 1

  • Dynamic 2

Parameters

  • Zone

    Zones available in the range of 0 to 23.

  • Ramp Rate.

    Ramp rate ranges from Instant, 4 sec to 17 mins.

These parameters are applicable for below functions:

  • Volume Up

  • Volume Down

  • Volume Cycle

  • Treble Up

  • Treble Down

  • Treble Cycle

  • Bass Up

  • Bass Down

  • Bass Cycle

  • Balance Left

  • Balance Right

  • Balance Cycle

  • Zone

    Zones available in the range of 0 to 23.

These parameters are applicable for below functions:

  • Next Source

  • Previous Source

  • Dynamic 1

  • Dynamic 2

  • Zone

    Zones available in the range of 0 to 23.

  • Source

    Zones with available levels ranging from 0 to 7.

These parameters are applicable for below functions:

  • Preset Source

Multi-Toggle

Allows to toggle multiple groups in an application.

Application

Each key can have 4 applications

By default, Lighting application is selected.

Groups

Each key has 8 Groups

Allows to select available groups in selected lighting application.

Allows to select available groups in selected enable application.

Linked

Allows add conditional logic behavior to a button press of a key.

IMPORTANT:

Linked widget will be disabled/hidden in the list when:

  • a linked widget cannot be selected/defined for the first /main widget of a key.

  • selecting a widget which is already defined as a Linked widget.

  • selecting a widget number which is already configured as a linked widget type and is assigned to any other Key.

Linked widget will be enabled in the list when:

  • an additional (second or more) widget added to the key (must add another widget to the key to use linked widget).

  • any widget number is already configured as a linked widget type and is not assigned in any other key.

NOTE: An additional (second or more) widget added to the key, widget already assigned to a key cannot be changed/modified to a linked widget. It can only configure a widget which is not assigned.

Once the linked widget is selected in a key, the widget number or widget type cannot be modified. The linked widget must be removed from the key and then added again.

Control Widget

  • Widgets that are already configured/assigned to the current key are displayed and allowed for selection.

  • While adding an additional widget to a key, and if the widget number selected is a control widget for an existing linked widget, then the associated linked widget also appears in the (to be added) key.

  • Removing the first/main widget in a key which is configured as a control widget for a linked widget in the same key displays a confirmation dialogue to confirm the action. On selecting YES, both the control and linked widgets are removed from the key.

    Click Yes to save the changes in widget and to delete linked widget.

    Click No to cancel the operation.

  • Selecting an existing linked widget for a key, the control widget property updates to reflect the first/main widget for that key.

  • The linked relationship between the linked widget and the control widget in all the keys and across all the profiles are maintained and displayed when:

    • A linked widget is added to a key.

    • A widget is changed/modified to a control widget.

NOTE: Once a control widget is selected, the control selection cannot be modified. The linked widget must be removed from the key and then added again.

Linked Event

Linked Event options include:

  • Control Widget Turns On

  • Control Widget Turns Off

  • Control Widget Timer Expiry

Linked Action

Linked Action options include:

  • Turn On

  • Turn Off

  • Preset

  • Turn On and Start Timer

  • Turn Off and Start Timer

  • Start Timer

  • Trigger Event

  • Enable Event

Group

Allows to select among existing groups.

Level/Expiry Level

Allows to set a level between 1 to 100%.

Ramp Rate/Expiry Ramp Rate

Allows to set ramp rate between 4 sec to 17 min, by default its instant.

Duration

Allows to set the duration in hh:mm:ss.

Disable link in this Profile

This property is applicable for all the linked widgets in the current profile. By default it is unchecked.

Checking Disable link in this profile will disable the linked widget in the current key.

The control widget continues to operate maintaining the linked widget relationship.

Property is disabled when profiles are not in use.

IMPORTANT:
  • The Disable link in this Profile property can be set only while using more than one profile in the device.

Indicator

Indicator Assignment

  • The indicator assignment property for the key is displayed only in an enabled state widgets that are not configured as a linked widget for user selection. Linked Widgets are disabled (appear in a disabled state).

  • If a valid widget is already defined for the Indicator Assignment property, then upon modification of the widget type, for that widget to a linked widget type, the Indicator Assignment property updates and selects automatically the first/main widget for the key.

Indicator On Color

Allows to set the indicator On color.

Indicator Off Color.

Allows to set the indicator Off color.

Indicators

Indicator Application

Allows to select among the defined Active Brightness control group and Idle Brightness control group.

Active Brightness

The Active Brightness can be equal to or greater than the Standby Brightness. By default set to 100%.

If a group is assigned to the Active Brightness Control Group, then the start up level for that group is the value set here.

Active Brightness Control Group

To control the active brightness, select the group

By default, <unused> is selected. Click to edit the group and to create new group.

Standby Timeout

The minimum value of 0 sec disables the Standby Timeout for this device.

Standby Brightness

The Standby Brightness can be equal to or less than the Active Brightness. By default set to 100%.

If a group is assigned to the Standby Brightness Control Group, then the start up level for that group is the value set here.

Standby Brightness Control Group

To control the idle brightness, select the group

By default, <unused> is selected. Click to edit the group and to create new group.

Nightlight Options

Profile

Allows the keys to change their behavior when triggered. Up to four profiles can be used.

Profiles utilize different widgets to define alternate (or same) key behavior for each profile.

All the profiles will be available. By default, profile 1 will be selected.

Enable Nightlight

Check the check box to enable nightlight.

Ignore First Key Press

This field is enabled only when Enable Nightlight is checked.

Nightlight Indicator Color

Nightlight Indicator color can be set to:

  • Off

  • 8 different colors

  • 2 user defined

  • 5 Dynamic (using C-Bus group to control)

NOTE: is enabled only for user and dynamic changes

Nightlight Color Control Group

Uses a C-Bus group to control the nightlight.

  • Level 0: Group is off

  • Above Level 0: Group is on

By default, <unused> is selected. Click to edit the group and to create new group.

Corridor Linking

Application

Select the application to be applicable for corridor linking.

Link Group

A common group address is assigned to all units sharing the same common area.

By default, <unused> is selected. Click to edit the group and click to create new group.

Corridor Group

The group address that is used for the common area that is adjacent to the office.

By default, <unused> is selected. Click to edit the group and click to create new group.

Office Group

The group address that is used for the Office which is adjacent to the common area.

By default, <unused> is selected. Click to edit the group and click to create new group.

Corridor Timer

Allows to set the timer for corridor timeout. By default, 00H: 05Min: 00s.

Error Reporting

Device ID

This field displays the unique Device ID for the device.

NOTE: The Device ID is for the entire device and is as same for measurement.

When you assign a Device ID, and then if you set the Device ID to Not Assigned, then all properties in both the Error Reporting and Measurement section are reverted to their default settings and disabled (grey out state).

Mouse over on the Device ID info icon to view the tooltip message.

Mode Control Group

This field allows to add an enable group (0–254).

If you assign a group, Regular Reporting Interval drop-down is enabled.

Regular Reporting

This field configures the Error Reporting mode of the Dimmers into one of modes:

  • Disabled (Triggered only)

  • All Errors, most recent and most severe

  • All Errors, most recent only

  • Minimum Errors, most recent only

  • Minimum Errors, most recent and most severe

Mouse over on the Regular Reporting info icon to view the tooltip message.

Regular Reporting Interval

This drop-down is used to select the time interval period between the completion of a regular report and beginning of the next report in Always On, Most recent only and Always On, Most recent and most severe modes. By default, the interval is 30 minutes

Regular reporting interval is enabled for all others except the Trigger Only mode.

Trigger Group

This field contains a Trigger Group to trigger an error reporting event for any of the three error reporting modes. When a Trigger group is created, resend and acknowledge action selector are displayed.

The Resend Action Selector is set to send all errors and Acknowledge Action selector is set to acknowledge all errors.

Destination Network

This field contains the destination C-Bus network to which the key units routes the error reporting messages. This allows the error messages to be sent to a remote C-Bus network for central monitoring if it’s not the local network

Mouse over on the Destination Network info icon to view the tooltip message.

Advanced

C-Bus Voltage Warning Set Threshold

  • By default, Disabled is selected.

  • The value selected must be less than the C-Bus Voltage Warning Clear Threshold value selected.

  • If the C-Bus Voltage Warning Clear Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Warning Clear Threshold value to (current C-Bus Voltage Warning Set Threshold value + 1 V).

Mouse over on the C-Bus Voltage Warning Set Threshold info icon to view the tooltip message.

C-Bus Voltage Warning Clear Threshold

  • By default, Disabled is selected.

  • The value selected must be greater than the C-Bus Voltage Warning Set Threshold value selected.

  • If the C-Bus Voltage Warning Set Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Warning Set Threshold value to (current C-Bus Voltage Warning Clear Threshold value - 1 V).

Mouse over on the C-Bus Voltage Warning Clear Threshold info icon to view the tooltip message.

C-Bus Voltage Critical Set Threshold

  • By default, Disabled is selected.

  • The value selected must be less than the C-Bus Voltage Critical Clear Threshold value selected.

  • If the C-Bus Voltage Critical Clear Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Critical Clear Threshold value to (current C-Bus Voltage Critical Set Threshold value + 1 V).

  • If the C-Bus Voltage Warning Set Threshold has a value set (other than Disabled), then the value selected must be less than current C-Bus Voltage Warning Set Threshold value.

Mouse over on the C-Bus Voltage Critical Set Threshold info icon to view the tooltip message.

C-Bus Voltage Critical Clear Threshold

  • By default, Disabled is selected.

  • The value selected must be greater than the C-Bus Voltage Critical Set Threshold value selected.

  • If the C-Bus Voltage Critical Set Threshold is Disabled, then setting a value here will also set the C-Bus Voltage Critical Set Threshold value to current C-Bus Voltage Critical Clear Threshold value - 1 V.

Mouse over on the C-Bus Voltage Critical Clear Threshold info icon to view the tooltip message.

Unit Over Temperature Set Threshold

This field is a combo box which is by default set to 70 °C.

The Unit Over Temperature Set Threshold property increments by 1 °C with a range of 1 °C - 80 °C.

Mouse over on the Unit Over Temperature Set Threshold info icon to view the tooltip message.

Unit Over Temperature Clear Threshold

This field is a combo box which is by default set to 65 °C.

The Unit Over Temperature Clear Threshold property increments by 1 °C with a range of 0 °C - 79 °C.

Mouse over on the Unit Over Temperature Clear Threshold info icon to view the tooltip message.

Measurement

Device ID

This field displays the unique device ID for the device.

NOTE: The Device ID is for the entire device and is as same Error.

Mouse over on the Device ID info icon to view the tooltip message.

Request Trigger Group

Select the trigger group for measurement application.

By default, <unused> is selected. Click to edit the group and to create new group.

Mouse over on the Request Trigger Group info icon to view the tooltip message.

Destination Network

This field contains the destination C-Bus Network to which the key units routes the error reporting messages. This allows the error messages to be sent to a remote C-Bus Network for central monitoring if it’s not the local network.

Mouse over on the Destination Network info icon to view the tooltip message.

Temperature Offset

Allows to set the device to offset between 25 °C to 25 °C.

Sensor Stabilization Delay

The Sensor Stabilization Delay is applicable to both the onboard temperature and humidity sensors only upon device power up.

The device will not send any Measurement data or raise any alarms until the delay time period has elapsed.

Sensor Stabilization Delay is set in H:M with 1 hour increment for hours and 1 minute increment for minutes. Maximum delay value that can set is 4:14.

Mouse over on the Sensor Stabilization Delay info icon to view the tooltip message.

Temperature Broadcast

Broadcast Interval

Allows to set the interval to broadcast temperature

By default Do Not Broadcast is selected.

Broadcast interval can be set between 10 seconds to 40 minutes.

Broadcast on Change Threshold

By default Disabled is selected.

Broadcasts if the unit crosses the set threshold.

Humidity Broadcast

Broadcast Interval

By default Do Not Broadcast is selected.

Broadcast interval can be set between 10 seconds to 60 minutes.

Broadcast on Change Threshold

By default Disabled is selected.

Broadcasts if the unit crosses the set threshold

Profile

Allows the keys to change their behavior when triggered. Up to four profiles can be used.

Profiles utilize different widgets to define alternate (or same) key behavior for each profile.

All the profiles will be available. By default, profile 1 will be selected.

Alarm Application

Select the application for alarm.

Temperature Alarms

Enable High Temperature Alarm

Select the check box to enable alarm on unit’s high temperature.

Alarm Group

Select the group for alarm.

By default, <unused> is selected. Click to edit the group and to create new group.

Enable Group

Select the enable group .

By default, <unused> is selected. Click to edit the group and click to create new group.

Enable Group Restore

This field is enabled only when Enable group is been selected.

Enable group can be restored in one of the following modes:

  • All events disabled (Default)

  • Only On events enabled

  • Only Off events enabled

  • All events enabled

Alarm Set Threshold

Set the alarm set threshold between 46 - 60 °C

Alarm Clear Threshold

Set the alarm clear threshold between 0 - 49 °C

Enable Low Temperature Alarm

Select the check box to enable alarm on unit’s low temperature .

Alarm Group

Select the group for alarm

By default, <unused> is selected. Click to edit the group and click to create new group.

Enable Group

Select the enable group

By default, <unused> is selected. Click to edit the group and click to create new group.

Enable Group Restore

This field is enabled only when Enable group is selected.

Enable group can be restored in one of the following modes:

  • All events disabled (Default)

  • Only On events enabled

  • Only Off events enabled

  • All events enabled

Alarm Set Threshold

Set the alarm set threshold between 0 - 14 °C.

Alarm Clear Threshold

Set the alarm clear threshold between 11 - 60 °C.

Humidity Alarms

Enable High Humidity Alarm

Select the check box to enable alarm on unit’s high humidity.

Alarm Group

Select the group for alarm.

By default, <unused> is selected. Click to edit the group and click to create new group.

Enable Group

Select the enable group

By default, <unused> is selected. Click to edit the group and click to create new group.

Enable Group Restore

This field is enabled only when Enable group is been selected.

Enable group can be restored in one of the following modes:

  • All events disabled (Default)

  • Only On events enabled

  • Only Off events enabled

  • All events enabled

Alarm Set Threshold

Set the alarm set threshold between 85 - 100 %RH.

Alarm Clear Threshold

Set the alarm clear threshold between 0 - 85 %RH.

Enable Low Humidity Alarm

Select the check box to enable alarm on unit’s low humidity.

Alarm Group

Select the group for alarm.

By default, <unused> is selected. Click to edit the group and click to create new group.

Enable Group

Select the enable group

By default, <unused> is selected. Click to edit the group and click to create new group.

Enable Group Restore

This field is enabled only when Enable group is selected.

Enable group can be restored in one of the following modes:

  • All events disabled (Default)

  • Only On events enabled

  • Only Off events enabled

  • All events enabled

Alarm Set Threshold

Set the alarm set threshold between 0 - 10 %RH.

Alarm Clear Threshold

Set the alarm clear threshold between 15 - 100 %RH.

Global

Unit Parameters

Status Request Interval

Allows to set minutes and seconds for status request interval.

Device Idle Time out

Allows to set minutes and seconds for status request interval.

Device Scenes

Displays the number of scenes used

Scene Manager.

Device Sequences

Displays the number of sequence used

Sequence Manager.

Device Key Assignments

Key Assignment Overview.

Unit Identification

Unit Type

This field contains the unit type of the device.

Catalogue Number

This field contains the catalog number related to the unit type.

Firmware Version

This field shows the version number of the C-Bus interface firmware which exists on the physical network or which has been assigned to a logical representation of the unit in the database

Part Name

This field contains the part name which is stored in the unit hardware, that can be modified.

Unit Address

This field displays the unit address assigned to the device.

Serial Number

This field contains the serial number which exists on the physical unit.

Tag Name

This field contains the name that user can give to the logical representation of the unit. This name can be up to 32 characters long and is stored in the project database only.

Notes

This field contains a location to add notes about the unit which is stored in the project database only.

Status

Status will be displayed only when the unit is live

C-Bus Voltage (V)

Displays the C-Bus Voltage.

Unit Humidity (% RH)

Displays unit’s humidity.

Unit Temperature (°C)

Displays unit’s temperature only when the Sensor Stabilization Delay time period is elapsed.

Once configuring relays are completed, click Save to save the changes.

Scene Manager

The Scene Manager allows to create, edit and manage scenes for selected C-Bus Device.

New scene items can be added to scenes using any of the available C-Bus group applications 1 to 4 defined for this device.

Some of the functions of scene manager is as demonstrated as below:

To edit the group name:

  1. Select the group and click Edit Group.

  2. Enter the new group name.

Clear Scene: Clear Scene clears all the scene items in the list irrespective of being selected.

Remove Scene: Remove Scene removes only the selected scene items from the list back to the group list. (can also remove scene by selecting scene and clicking )

Sequence Manager

The Sequence Manager can create, edit and manage sequences for the selected C-Bus Device. New sequence items can be added to sequences using the available Action types and configured separately.

Some of the functions of Sequence Manager is as demonstrated as below:

Clear Sequence: Clear sequence clears all the scene items in the list irrespective of being selected.

Remove Sequence: Remove sequence removes only the selected scene items from the list (can also remove scene by selecting scene and clicking )

Action Types

Sequence Items

Delay

Time: Allows to set the delay in M:S

Lighting

Group: Allows to select from defined application.

Level: Allows to set the level value

Setting the Level value will automatically update the Percentage value.

Percentage:

Setting the Percentage value will automatically update the Level value.

Ramp Rate: Allows to set the ramp rate between 4-17 min. By default it is instant.

Trigger

Trigger Group: Allows to select from available Trigger groups in Application.

Action Selector: Allows to select from available Action Selectors in selected Trigger group.

Enable

Enable Group: Allows to select from available Enable groups in Application.

Value: Allows to select from available Enable Values in selected Enable group.

Security

Arm Mode

The different arm modes are:

  • Away mode

  • Night (home) mode

  • Day mode

  • Vacation mode

  • Highest possible

Lighting Label

Label: Allows to define max. 8 labels, edit label name and duplicate the labels.

Groups: Allows to select from defined application.

Language: English (By default and the only language).

Variant: By default has value 1, and ranges from 1 to 4.

Scene Trigger Label

Trigger Group: Allows to select from predefined Trigger Group, or add a new by editing the name.

Action Selector: Allows to select from predefined Action Selector, or add a new by editing the name.

Audio

Zone: Zones available in the range of 0 to 23.

Action: Allows to choose action between:

Set Volume to Level Provided.

Volume: Allows to set volume between 0 –100%.

Ramp Rate: Ramp rate ranges from Instant, 4 sec to 17 mins.

Set Source to source Provided.

Source: Zones with available levels ranging from 0 to 7.

Media Transport

Media Link Group: Address selection range limited to 0 to 31.

Action: Allows to choose action between:

  • Set Power

  • Set Shuffle

  • Set Repeat

  • Set Motion

  • Set Category: Value ranges from 0 - 127. By default, value is 0.

  • Set Selection: Value ranges from 0 - 32767. By default, value is 0.

  • Set Track: Value ranges from 0 - 16777215. By default, value is 0.

To: Allows to choose operation for selected action from the below options:

  • Power Off

  • Power On

  • Shuffle Off

  • Shuffle On

  • Repeat Current

  • Repeat Off

  • Repeat Track

  • Stop

  • Play

  • Pause

  • Resume

Key Assignment Overview

The Key Assignment Overview window displays a high-level view of the Widget/Function to key mapping per Profile.

  • Window allows to select each profile as desired (1 to 4).

  • The key layout of the window displays the list of keys in the order of 1 to 6 from left to right, and then top to bottom.

NOTE: Each key has a list of widget summary depending on the widget type.

Widget Type

Functions

Properties

Content

Lighting

All

  • Widget Type

  • Function

  • Group

  • Name of Widget Type

  • Name of Function (All Functions)

  • Group as configured in Widget (by name)

Timer

Shutter Relay

Enable

Fan Cycle

Audio

Linked

Multi Toggle

Scene

All

  • Widget Type

  • Function

  • Trigger Group

  • Action Selector

  • Name of Widget Type

  • Name of Function (All Widget Functions)

  • Trigger Group as configured in Widget (by name)

  • Action Selector as configured in Widget (by name)

Sequence

If a key is configured with more than one widget, the key displays UP/DOWN arrows for the user to cycle through all the widgets configured to the key.

The widget configuration for all keys across all profiles is visible. By default, (if a key is not configured) the Key displays the Lighting widget type and <Unused> function with the following default properties:

  • Widget Type – <Unused>

  • Function – <Unused>

  • Group – <Unused>

The data/information displayed in the Key Assignment Overview dialogue window is read-only.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.