Software Version 2.14.0

Inbuilt C-Bus Power Supply

SpaceLogic C-Bus Commission allows to enable/disable the "Inbuilt C-Bus Power Supply" function for the C-Bus Voltage Free Relays and Digital Dimmers.

NOTE: Enabling/Disabling C-Bus Power Supply from front panel of the respective device is also possible, refer respective Device User Guide.
  1. Select a relay/dimmer unit.
  2. In Properties window, go to Global > Inbuilt C-Bus power supply

    NOTE: Option is available only if:
    • The C-Bus network is opened and scanned.

    • A device is fully/partially matched.

  3. Check the check box to enable ‘Inbuilt C-Bus power Supply’. Confirmation message is displayed.

    Confirm Yes

    NOTE: Uncheck the check box to disable ‘Inbuilt C-Bus power Supply’ (By default, it is disabled). Confirmation message is displayed.

  4. Confirm Yes. If device configuration process is successful, below message is displayed.

    NOTE: If the device configuration process is failed, below error message is displayed.

  5. The enabled ‘Inbuilt C-Bus Power Supply’ for a respective device is visible in Network Device section as shown below.

    The icon represents ‘Inbuilt C-Bus Power Supply’ is been enabled for the device.

IMPORTANT: If the power supply enabled device is been removed from the live network and is re-added to the network, the network would be already enabled displaying following message .

If the device configuration reverting to previous settings is failed, below error message is displayed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.