Software Version 2.14.0

C-Bus Applications

The Application section window allows the management of the applications within a network. An application is used with a Group Address to define the relationship between devices. Example: which input(s) will control which output(s).

NOTE: C-Bus Application section is displayed in the Workspace window.

NOTE: Lighting, Trigger and Enable are the default applications added to all the networks in a project.

Application

Decimal

Hexadecimal

Lighting

56

38

Enable

203

CB

Trigger

202

CA

Error

206

CE

Measurement

228

E4

Emergency Exit Light

238

EE

Audio

205

CD

Media Transport

192

CO

Operations on C-Bus applications:

Add Applications

The Applications section allows the user to add an application to a network.

Prerequisites: A network must already be created in a network .

  1. Select a network from the Explorer window

  2. Click Applications

    Step result: The Application section is displayed in the Workspace window.

  3. Click Add Applications in the Workspace window

  4. Fill in the Mandatory fields

    Click Create

    An Application is created Successfully.

View content of an Application

Prerequisites: A network must already be created in a network and application must be existing.

  1. Select a network in the EXPLORER window.

  2. Click drop-down.

    All the applications in the network are displayed.

    NOTE: By default Lighting, Enable and Trigger applications are listed.
  3. Select the application to view content

The content of the Applications is displayed.

Edit Application

Prerequisites: A network must already be created in a network and application must be existing.

The edit application feature allows the user to modify the description of the application.

  1. Select a network in the EXPLORER window.

  2. Select an Application.

    NOTE:
    • The default applications cannot be edited.

    • Only Name and Description of an application can be modified.

  3. The process to edit an application is demonstrated below:

The application is modified.

Copy and Paste an Application

The SpaceLogic C-Bus Commission software allows the user to copy and paste the contents of an application from one network to another.

Prerequisites: A network must already be created in a network and an application must already be added in a network.

  1. Select a network from the EXPLORER window (a network form which an application has to be copied).

  2. Click .

    The process to copy and paste an application is demonstrated below:
  3. The content of the application is copied from one network and pasted in another network.

    NOTE: Performing paste operations on reserved applications and modifying their names are not allowed. Attempting the function will display the Resolve Conflict window, where neither the address nor the name can be modified.

Search an Application

The application section allows the user to search for an application or contents inside the application

Prerequisites: A network must already be created in a network and application must be existing.

  1. Select a network in the Explorer window

  2. Enter the application name in the search bar

    NOTE: This feature can also be used to search group addresses inside an application.

    If the search word includes the application name then the resulting applications that match will be displayed. If the search word includes a group address name then the resulting applications where that group address name exists will be displayed.

Sort Applications

Prerequisites: A network must already be created in the project and more than one application must be existing in a network.

The existing applications can be sorted using

Choose an appropriate option.

Delete an Application

The SpaceLogic C-Bus Commission software allows the user to delete an application in the network.

Prerequisites: A network must already be created in a network and application must be existing.

  1. Select a network from the Explorer window

  2. Click Applications

  3. Select an application from the workspace window to be deleted in the network

  4. Click

    The application is deleted from the network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.