Software Version 2.12.0

Sort Audio Zones

Prerequisites: The Audio Zones must already have been created in the Audio application.

The existing Audio Zones in an application can be sorted.

  1. Select the Audio Zone.

    NOTE:
    • A single audio zone can be chosen by selecting the check box of the required group, whereas all audio zones can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one audio zone, then hold down the SHIFT key and select on additional audio zones (grid) using the mouse.

    • For random multiple selection, select one audio zone, then hold down the CTRL key and select the next audio zone (grid) using the mouse.

  2. Click in the Zones section.

    The available sort methods are displayed.

  3. Select the appropriate sort method. The audio zones list will be sorted according to the selected sort method.

  4. Select anyone Zone and then select anyone function in the Functions : Zone section.

    Only when you select anyone Zone, the Function section is enabled.

    NOTE: You can select only one function at a time. The moment you select the function, the Levels section will be enabled.
  5. Select the Level.

    NOTE:
    • A single level can be chosen by selecting the check box of the required group, whereas all levels can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one level, then hold down the SHIFT key and select on additional levels (grid) using the mouse.

    • For random multiple selection, select one level, then hold down the CTRL key and select the next level (grid) using the mouse.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?