Software Version 2.14.0

Copy Action Selectors

The Action Selectors created in a group can be copied to another Trigger group in the same Trigger application on same network or from the Trigger application from a different network in the project.
Prerequisites: The Action Selector must already be copied from a Trigger Group.
  1. Go to Applications > Trigger.
  2. Select the group check box in the Trigger Groups section. The Action Selectors for the selected Trigger Group are displayed in the Action Selectors section.
  3. Select the required Action Selectors and click in Action Selectors section.
    NOTE:
    • A single action selector can be chosen by selecting the check box of the required action selector, whereas all action selectors can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one action selector, then hold down the SHIFT key and select on additional action selectors (grid) using the mouse.

    • For random multiple selection, select one action selector, then hold down the CTRL key and select the next action selector (grid) using the mouse.

    • The icon will be disabled, if an action selector is not selected.

    Step result: The selected action selectors are copied.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.