Software Version 2.14.0

Edit Action Selector

Prerequisites: The Action selectors must already be existing in the selected Trigger group of Trigger application.

  1. Double-click on the Action selector l name that has to be edited/renamed

    Step result: Edit Trigger Group dialog box is displayed.

  2. Edit the Action selector name and click OK.

    NOTE: Special characters /,”,# and maximum of 32 characters in the Action selector name is valid.

    Step result: The Action selector name is updated.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.