Software Version 2.14.0

Audio Application

The Audio Control application control the audio levels such as volume, bass, and treble as well as the selection of audio sources for zones.

The Audio application is responsible for the control of audio levels such as volume, bass, and treble as well as for the selection of audio sources for Audio Zones as defined within the Audio application.

Audio application is created using a reserved application number 205.

Audio Zones and control options for the Audio application can be configured in C-Bus devices such as:

  • The new generation C-Bus wall plate devices (key input units).

  • The C-Bus eDLT key input unit.

  • The C-Bus Multi Room system (Matrix Switches and Amplifiers).

  • The C-Bus Home Controller.

  • The C-Bus Automation and Application Controllers (for control of third party audio systems).

The procedure to create a audio application is as demonstrated below:

NOTE: To resolve the paste conflict of an application click here

Operations performed in Audio application

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.