Software Version 2.14.0

Delete Error Object

Prerequisites: Error application must already have been created in network and error object must have been added.
  1. Select the error object.
    NOTE:
    • A single error object can be chosen by selecting the check box, whereas all error objects can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one error object, then hold down the SHIFT key and select on additional error objects (grid) using the mouse.

    • For random multiple selection, select one error object, then hold down the CTRL key and select the next error objects (grid) using the mouse.

  2. Click in the Device Channel List and Error Details section.
    A Confirmation pop-up is displayed.
  3. Click Yes to delete the channels and No to cancel the delete operation.
    TIP: Alternate method to delete selected error objects is, right-click on the selected Device > Delete.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.