Software Version 2.14.0

Workflow of the software

A C-Bus and DALI installation can be programmed in various methods. The workflow defines a possible procedure.

  1. Create a new project and fill in the project information in the required fields, see Create project

  2. Create and add networks as per project requirement, see Add networks

    NOTE: Each project can have a maximum of 255 networks.
  3. Add devices to the network from Library window, see Library Window

    NOTE: If C-Bus DALI-2 Gateway has been added to the project, the DALI devices must be added into the DALI lines.
  4. Create applications, see Add applications

  5. Add group address information to applications from C-Bus Application section.

  6. Set properties for the devices using the Properties window, see Properties window

  7. Open and scan the C-Bus network and the DALI line if required, see Network Devices

    Result: The software searches for the devices in the network.

  8. Identify the DALI-2 devices in the network using Auto Identify or Identify functions.

    NOTE: If the C-Bus devices are already addressed, then this step is not required. Verify the flashing lights in the physical device.
  9. Extract the fully matching devices from Network Devices to Devices in Project section, see Extract devices

  10. Deploy each configured/reconciled device to the network, see Deploy device to network

    Result: The device information is displayed in the Deployment Queue window.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.