Software Version 2.12.0

Sort Media Link Groups

Prerequisites: The Media link groups must already have been created in the Media Transport application.

The existing Media Link Groups in the application can be sorted.

  1. Select the Media Link Group.

    NOTE:
    • A single media link group can be chosen by selecting the check box of the required group, whereas all media link groups can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one media link group, then hold down the SHIFT key and select on additional media link groups (grid) using the mouse.

    • For random multiple selection, select one media link group, then hold down the CTRL key and select the next media link group (grid) using the mouse.

  2. Click in the Media Link Groups section.

    The available sort methods are displayed.

  3. Select the appropriate sort method. The Media Link Group list will be sorted according to the selected sort method.

  4. Select anyone Media Link Group and then select anyone function in the Functions : Media Link Group section.

    Only when you select anyone Media Link Group, the Functions section is enabled.

    NOTE: You can select only one function at a time. The moment you select the function, the Levels section will be enabled.
  5. Select the Level.

    NOTE:
    • A single level can be chosen by selecting the check box of the required group, whereas all levels can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one level, then hold down the SHIFT key and select on additional levels (grid) using the mouse.

    • For random multiple selection, select one level, then hold down the CTRL key and select the next level (grid) using the mouse.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?