Software Version 2.14.0

Delete Measurement Data

Prerequisites: Measurement application must already have been created in network and measurement details must have been added.
  1. Select the measurement data.
    NOTE:
    • A single measurement data can be chosen by selecting the check box, whereas all measurement data can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one measurement data, then hold down the SHIFT key and select on additional measurement data (grid) using the mouse.

    • For random multiple selection, select one measurement data, then hold down the CTRL key and select the next measurement data (grid) using the mouse.

  2. Click in the Device Channel List and Measurement Details section.
    A Confirmation pop-up is displayed.
  3. Click Yes to delete the channels and No to cancel the delete operation.
    TIP: Alternate method to delete selected measurement data is, right-click on the selected Device > Delete.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.