Software Version 2.12.0

Sort Measurement Data

Prerequisites: The measurement details must already have been created in Measurement application.

The existing measurement details in the application can be sorted.

  1. Select the measurement data.

    NOTE:
    • A single measurement data can be chosen by selecting the check box, whereas all measurement data can be chosen by selecting the check box on the top.

    • For range (sequential) selection, select one measurement data, then hold down the SHIFT key and select on additional measurement data (grid) using the mouse.

    • For random multiple selection, select one measurement data, then hold down the CTRL key and select the next measurement data (grid) using the mouse.

  2. Click in the Device Channel List and Measurement Details section.

    The available sort methods are displayed.

  3. Select the appropriate sort method. The measurement data list will be sorted according to the selected sort method.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?