Software Version 2.14.0

Trigger Application

The Trigger application is widely used across C-Bus to trigger actions or events such as C-Bus lighting scenes or to start an irrigation program.

The Trigger application contains functions for editing the application and related trigger compatible trigger groups. Each of the Trigger Group and Action selector entry contains information in the fields.

When a network is created in project, the Trigger application is created by default with an application number 202.

The Trigger application is widely used across C-Bus to trigger actions or events such as C-Bus lighting scenes or to start an irrigation program.

The Trigger application is viewed similar to lighting application, click here

For more details, click:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.