Software Version 2.14.0

Emergency Exit Light Application

Prerequisites: The network must have already been created in the project .

Emergency Exit Light application is created using a reserved application address 238.

SpaceLogic C-Bus units which supports Emergency Exit Light application are:

  • DALI ECG DT 1 (Generic): Emergency or Exit Light (Generic)

  • DALI ECG DT1 A: Emergency or Exit Light (Switched Maintained Dimmable)

  • DALI ECG DT1 B: Emergency or Exit Light (Switched Maintained Non-Dimmable)

  • DALI ECG DT1 C: Emergency or Exit Light (Maintained)

  • DALI ECG DT1 D: Emergency or Exit Light (Non-Maintained)

The procedure to create an emergency exit light application is similar to other applications with a reserved address 238.

For more details:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.